Hi,
Can you please provide an estimate of the variation in open loop gain at 1Khz for OPA172 over operating temperature (-55 to 125C).
The load seen by the amplifier is 23mH+310ohm.
Thanks,
Shihab.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please provide an estimate of the variation in open loop gain at 1Khz for OPA172 over operating temperature (-55 to 125C).
The load seen by the amplifier is 23mH+310ohm.
Thanks,
Shihab.
Hello Shibab,
I did some investigation into your question about how the OPA172 open-loop gain (Aol) will vary with the 23 mH + 310 ohm load, over temperature. Here's my conclusions:
Using this range of Aol variation would allow the closed-loop gain (Acl) to be calculated over temperature, etc.
The Op Amp Bandwidth sessions of the TI Precision Labs series may be referenced if additional information on the subject of GBW is needed:
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
Thanks you for the reply.
From you post what I understand is over the operating temperature -55 to +125C, the estimate for Aol variation at 1Khz is 74dB to 83dB. Typical is 80dB.
Can we consider the Aol value at -55C will only be in increasing order than the Aol at 25C?
Also the Aol at +125C will only be in decreasing order than the Aol at 25C?
I thought a tolerance analysis will be more meaningful if we can consider the actual behavior of Aol at -55 and 100C, than considering the above specified Aol variations at both temperature extremes.
Also, can you please provide any white paper you have on the subject "Opamp Aol variation over temperature"?.
Thanks,
Shihab.
Hi Shihab,
The short article below describes the changes in an op amp's Aol and open-loop output impedance (Zo) over several operational factors, including temperature.
The results show that at lower temperature the device features a higher unity-gain bandwidth and higher low-frequency Aol value than while operating at high temperatures. The article is based on a typical 3-stage CMOS device and some other types of devices may behave differently.