Hi,
I would like to ask you a basic question about input offset voltage.
According to the datasheet, Vos = 10uV(Max) @ 25℃ and offset drift is 0.05uV/℃.
In case of Vos is 10uV @25℃ now, when the temperature is going to 125℃, the Vos is going to 15uV (10+0.05x100=15).
That is to say, Vos(Max) is 15uV @-40 to 125℃.
Is this correct?
Thank you for your support.
Best Regards,