[ AMC1301 ] Relation between Bias Current, R4/R5 and Gain
Hi,
Can you help me to understand the relation between bias current and Gain?
From the drawing and description in the datasheet, I understand that the bias current can be calculated with the equation below.
Vcm = (R4 + R5 ) * Ibias
Where
Vcm = 2V
R4 = 12.5kohm
Ibias = -60uA
So R5 = 20.8kohm.
WIth these estimation, the graph can be correctly obtained. Is this understanding correct?
Here, another point, I cannot understand is the gain.
The gain of AMC1301 is fixed 8.2. I would imagine that the combination of R4 and R5 shows the indication of this gain, however not...
As far as I check the datasheet of AMC1305, it seems that there is a relation between R4/R5 and gain.
Can you help me to understand this correctly?
Thanks,
Ken