Hello there,
My customer is having a hard time determining how fast the OPA2330 turns on. Where can he find that information? Their product currently works using the MCP6002 from Microchip. They are looking to improve the current rating of this part which is 100uA/channel. Can someone recommend other low power options to the OPA2330 to replace the MCP6002 in this application.
My customer is having a hard time determining how fast the OPA2330 turns on.
Where can he find that information?
Their product currently works using the MCP6002 from Microchip. They are looking to improve the current rating of this part which is 100uA/channel. Can someone recommend other low power options to the OPA2330 to replace the MCP6002 in this application.
Their product currently works using the MCP6002 from Microchip. They are looking to improve the current rating of this part which is 100uA/channel.
Can someone recommend other low power options to the OPA2330 to replace the MCP6002 in this application.
Here is what the customer needs:
Dual, 5Vin, rail to rail. Has to be on and settled within 2mS of power up.