• Resolved

AMC1100: AMC1100

Part Number: AMC1100

Hello,

My requirement is to monitor the 120V AC power supply when the load(1500Watt Heater) is connected and maintained the power level when there is variation in input range(110 VAC to 125VAC). I am trying to build a circuit which can deliver below result:

Input current Delta = 1.63 Amp(Rms)

Vout= 0-5VAC (pk-pk)

I thought of using an AMC1100 amplifier. can anyone suggest which approach would meet my requirement?

Regards

Rajesh