Other Parts Discussed in Thread: OPA1622
Hi, i'm working with a OPA197 outputting a sine wave centered in zero with 1.76Vp , ie, 1.250 Vrms. The amplifier is powered with +-3.3V and i was expecting to get something close to a maximum source current of a Irms= 46mA (65mA peak as stated in the datasheet) but it turns out if i put a load that forces a current higher than 30mA, the amplifier doesn't provide it and it starts to clip the wave. Am i missing something ? Thank you.