This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1100: IEC61010-1

Part Number: AMC1100

Hi,

I have a design that uses the AMC1100DWV to measure mains voltage. I am having difficulty getting it through IEC61010-1. As far as I can see it is approved for use for edition 2 of the standard but not edition 3. I am aware of white paper slyy055 but our test house says this is just an opinion and they need a certificate.

Do TI intend to get this part certified to IEC61010-1 3rd Ed and if so when?

Thanks,

Mike

8 Replies

  • Hi Mike,

    With the AMC1100, there are some exceptions to consider for compliance to 61010-1 3rd edition. Let me talk with our compliance contacts and see what we can do here.

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    Hi Mike,

    The AMC1100 is listed under VDE 0844-10, so that should be enough to satisfy your test house.  The certificate is here:

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    It seems that the AMC1100 provides basic insulation but not reinforced insulation, so we can't use it. The unit it is going in is earthed so I don't understand why it need reinforced insulation but that's what I have been told.

    Mike

  • In reply to Michael Forster:

    Hi Mike,

    Your AC Mains voltage should be the driving factor for determining basic versus reinforced isolation levels.  If you used the AMC1100 in the DWV package, the AMC1301 would be a drop in replacement and is qualified to reinforced voltage levels.

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    Hi Mike,

    Is the AMC1301 going to work for you?

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    Hi Tom,

    It seems not. The problem seems to the DTI, Distance Through Insulation, which is given as >= 0.027mm but for IEC/EN/UL/CSA 61010-1 3rd edition Clause 6.7.2.2.2, 0.4mm is required, or Clause 6.7.2.2.4 for multiple layers of thin-film.

    Your slyy055 white paper says -

    TI has initiated the certification process of all its products to help end-equipment manufacturers
    meet these requirements. VDE and TÜV have completed the certification process for many of TI’s isolation devices
    and several product families are CSA-certified now, with the remainder scheduled to be certified

    Is the AMC1301 now certified to edition 3 or is it scheduled to be?

    Mike

  • In reply to Michael Forster:

    Hi Mike,

    The SLYY055 document was put together by one of the guys here at TI who deals with the digital isolators, devices like the ISO7421. Some of those isolators have been tested to certain aspects of the IEC 61010 standard, but the AMC1100 and the AMC1301 have not been.  The parts should still be qualified through section 14 though at the component level.  If it's OK with you, I'll contact you directly and we can talk more about your specific application.

     

    Regards,

    Tom

  • In reply to Tom Hendrick:

    I am simply trying to measure the mains voltage and feed the value into a micro so sure, give me a call.

    Mike

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.