Other Parts Discussed in Thread: OPA1644, BUF634, , PCM1792A, OPA1622, OPA1612, OPA1688
I was interested in using the OPA627 (and maybe a BUF634) as the output stage of my DAC/headphone amp. I plan on using the OPA1644 as the Trans-impedance amplifier to convert the current from the PCM1792A DAC to a differential voltage this signal into a single OPA627 (one each for left and right) configured as a difference amplifier with a gain of 1 to convert the signal to a signal ended signal to drive a pair of headphones (50 ohms to 600 ohms).