hi all,
I need an amplifier to measure the nA/pA level current. do u have some recommend amplifier?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi all,
I need an amplifier to measure the nA/pA level current. do u have some recommend amplifier?
thanks
Hi Zhenhua,
We can not make a recommendation without more information about your application. For example:
1) What is the full scale range of current you need to measure? Will this current always be nA to pA?
2) What are you measuring the current of? What is the system load? Are you intending to do a high-side or low-side current measurement and if high-side, what is the voltage of your system source?
4) What supplies do you have available and what kind of output range do you need?
The more information you can share the better we can assist you.
Regards,
Zak Kaye
hi Zak,
thank u for your reply, following is my application information
1、the current range is 1nA~1uA
2、what i measure is a small corrosion current of a corrosion probe, like a primary battery,i just measure the current between the positive and the negative pole, and the voltage between the two poles is less than 0.5V.
3、I would like to use a two stage amplifier and I already choose ADS1216 for the AD convertion, so the max output voltage will be 2.5V
thanks
hi all,
could you give some recommendation about the choice of amplifier &the circuit
thanks