Other Parts Discussed in Thread: ADS1220, INA827, INA826, OPA202
Hi there,
I need a low cost alternate to AD8220 INA of Analog Devices. So, I'm planning to use INA114 to amplify the input signal with gain around 20 while the bipolar differential input signal will be in the range of 70µVp-p to 5mVp-p. I need minimum CMRR to be 100dB or 120dB will better on DC to 60 Hz with low offset voltage & drift.
My aim is to design a low cost Electromagnetic Flow meter.
Can INA114 be used as an alternate to AD8220?
If yes,
Since I'm using ADS1220 ADC and this doesn't allow me to pull out the internal band gap reference. Can I connect reference pin of INA114 (i.e. Pin No. 5 of 8-Pin DIP) package to a 1M resistor voltage divider with supply 5V (~2.5V at REF Pin with a parallel coupling capacitors of 10µF & 0.1µF for noise suppresion)?
else,
Can you suggest me good low cost alternate INA?
You can visit for brief detail of my application.
Thanks & Regards,
Harish