Hi team,
The customer is using XTR108. The current source output is configured to VI-0.
When the EEPROM data is not written, there is no current output. When the customer writes the EEPROM data,
VI-0 can output 2mA current. And the 2mA current remains the same even if he changes PGA parameters or the input signal.
The sensitivity of the resistance bridge sensor is 2mv/v. The input differential voltage of the resistance bridge sensor is 0~10mV.
The input common voltage of the resistance bridge sensor is 2.5V.
The attach is the customer's schematic and his EEPROM data.
Would you provide some suggestions for the customer' issue?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments