Hi,
I have a question about OPA388.
Is there data of Voltage Noise at 200kHz?
I'd like to confirm whether it has some spurious at 200kHz.
Best Regards,
itabi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Itabi,
Below plase see a raw data showing OPA388 input voltage noise spectral density up to 10MHz. In the graph you may notice the variation in the peak-to-peak values caused by changing gains at f=10kHz and f=100kHz. A chopper noise can be seen at around 200kHz mark and the charge pump noise past the 10MHz.