This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6321: about LMH6321 power supply

Part Number: LMH6321

hi dear supporting team,

customer is using TPS7A801 to supply 5V for LMH6321, with 10uF,0.1u,1nF bypass cap close to the pin, and also a ferrit bead of 150Ohm in seriers.  there are around 50% brds have 28kHz glitchs at the output of LMH6321, if change the power supply of LMH6321 to external DC-DC, then there is no such issue.  from some experiment we think it is some reasonance btw the power supply pin of LMH6321 and TPS7A801,  we triied more bypass cap btw them, while no improvement. and the TPS7A801 also  be power supply for some other amp, it seems has no such issue. the load of LMH6321 is a switch,  so for LMH6321 power supply , if the loading is heavy, is there any more effort we could take?  tks a lot!

  • Hi Vera,

    With the bypass cap, are you using multiple caps of different sizes in parallel or one large cap? Also, you could possibly try adding a small series resistor on the power supply line to the part. if it is indeed a resonance a small resistance may help to dampen it.

    Regards,