Other Parts Discussed in Thread: AMC1200, AMC1311, PMP9480
Hi everyone.
This is Mike and I want to thank you all for your support , and here is the next situation:
I want to measure the output of a three phase generator that has Wye conection. Just I'll take two phases and that is for monitoring the voltage and the frequency of that signal. I've searched about techniques to measure high voltages and I found the AMC´s family of OpAmps. I think is a little easier when one has to measure a large signal with a constant voltage and frequency (here, at México, 127Vrms , 60 Hz) but in this application, the signal varies and just I want to make sure that the design will work. I can´t measure yet because my material has doesn´t arrived, I think it will be here in ¡ 3 Weeks !
The datasheet says the max Vin is 250mVpp so I design a voltage divider that at 600V and here is the result
When the input is at 50 Vrms, I'll have at the output 18 mV, the question is if at that level the AMC1200-Q1 Does still work so fine at the output?