Other Parts Discussed in Thread: LM27762, IVC102
Are there known issues operating this chip with +/- 2.5V supplies instead of a single rail 5V supply? I assumed it would work with dual rails provided the total differential voltage was within limits, but now I'm not so certain.
My supplies come from a LM27762, and I am seeing a lot of noise on the output of the LMP7721 that has been amplified from the supply rails. The PSRR spec of 92dB is specified for a single rail supply, and it has made me question if attempting to use dual rails is the source of the trouble. I'm using the LMP7721 as a current integrating preamp in the following configuration, so the gain is fairly substantial: