The output that I get at pin 4 & 7 is always 0.3 V. However, when I measured it at pin 3, I get the right result. Can You also check my values for the high and low frequency circuits.Low Tach & High Tach circuits.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The output that I get at pin 4 & 7 is always 0.3 V. However, when I measured it at pin 3, I get the right result. Can You also check my values for the high and low frequency circuits.Low Tach & High Tach circuits.pdf
Hi Isaam,
The three LM2907 devices shown in the NEW OUTPUT schematic attachment have their TACH+ inputs connected together at the left side connection of C17, but there isn't any resistance from that circuit node to ground (as Kai questioned). The TACH+ input (pin 1) needs a dc path to ground. It serves as a base current path when the PNP transistor on the TACH+ input side is required to turn on. I suspect the voltage on that input is never getting to ground at any point of the input drive cycle, and the LM2907 input comparator is not flipping state. You could monitor the input voltage waveform of the three LM2907 inputs with a DSO and observe what it looks is doing.
Or - try connecting a resistor (several kilohms) from the LM2907 TACH+ inputs to ground and see if the device begins to function. Some experimentation with the resistor value may be required.
Regards, Thomas
Precision Amplifiers Applications Engineering
I did place a resistor between TP10 and 5VCOM but it didn't work. I am also running into an issue with my High Tach and Low Tach circuits. Thanks