Other Parts Discussed in Thread: MULTI-CAL-SYSTEM, PGA309
Hello,
I have a UUT with a pre-gain of ~ 14.33 and a post gain of 2,
input stimulus voltages at the input to the 308 are calculated:
0.0856 Volts (for high stimulus) ( 3.25V target output voltage)
0.01433 Volts (for low stimulus) ( 0.75V target output voltage)
The two PGA308 sample boards work great with out settings.. i.e.
the % Error is 0.008%
But For some reason, we over shoot on the pre-calibration stage with out UUT
i.e. during the adjustment, the output voltage is higher then our target voltage by > 5%!
0.085998 |