Other Parts Discussed in Thread: LM7705
Hello,
I have a generic question about opamp functionality, but for my application I am using a OPA333. I intend to read the voltage across a shunt resistor and I am wondering about the limitation of the output voltage swing, namely the lower value threshold (i.e. VOL in datasheets). I am supplying the OPA333 between 5V and GND. According to datasheet the VCM range is -0.1<Vcm<5.1 and the output swing interval is 0.05<Vo<4.95. The shunt resistor has a value of 0.03Ohm and teh minimum load current is 0.35A resulting in a minimum sensed voltage of 0,0105V (no errors considered). At this input voltage I am violating the output voltage swing requirement (considering a voltage follower configuration) and probably my output will be limited around the VOL limit of 0.05V (worst case), which does not reflect the reality. My question is how the lower output voltage threshold will afect my output if I set a gain to my voltage follower stage (i.e. change it to a non-inverting amplifier; e.g. Av=15). Any explanation or literature suggestion is very wellcome.
Also in the datasheets I observed the output voltage swing is given for a device supplied between Vs and GND with the output Vo = Vs/2, 10kOhm load between Vo and Vs/2 (wich technically means no voltage across load resistor). Could you please explain how this is defined and what practically this means!?
Many thanks for your support,
Florin