Other Parts Discussed in Thread: ADS8688A, AMC1301, ISO124, PGA205, PGA203, PGA206
Hello,
I am using PGA281 for sensors data amplification.
There are various types of sensors.
Pressure sensors(Vout max 20 mVpp),Load cell(Vout max 20 mVpp),DC accelerometer(Vout max 2 Vpp) & Vibration sensors(Vout max 5 V).
Sensors Bw will be 5 KHz max.
Sensors output impedance will be less than 300 ohm.
I am using ADS8688A for data acquisitions from these sensors.
I need appropriate isolator at input side of signal conditioning befor PGA281. Please suggest??
For covering full dynamic range of ADC, i need higher gain so i am integrating this PGA281 with AD8421.