Other Parts Discussed in Thread: OPA2614,
Hello sir,
We are looking for a dual channel VGA splitter (1 x 2 ) with the following spec:
- Input signal: RGB
- Resolution: 1280*1024 @ 60Hz ( Bandwidth: 160MHz )
The THS7373 is suitable for this above application ?
For getting two VGA output how many IC need to use in this application?
Whether One IC is enough to drive two VGA outputs or Two IC required?
Thanks & Regards
Lakshmanan V