Hi TI and All,
I have designed XTR111 ckt. for 4mA to 20mA output. It is working fine. But I am facing issue regarding Error flag Output Pin. I have attached fig. for better understanding of ckt.
Observation: EF pin continuously low in the presence of Output load as well. So voltage at Gate of P MOSFET is 0V. And MOSFET is ON . So LED aslo continuously ON. But I want LED should be OFF when Load is connected at output and ON when load is disconnected.
MOSFET Specification : P-Channel MOSFET -60V Vds 20V Vgs SOT-23,OTR- -55C to +150C
So I hope you have understand my problem, hoping for positive reply ASAP.
Prashant