This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2376: About V- voltage

Part Number: OPA2376
Other Parts Discussed in Thread: OPA4376

Hi,

Could we input -5V for V-(Pin:11) and 0V for V+(Pin:4) ?

Best Regards,

Toshiyuki

  • Hi Toshiyuki,

    yes, if you shift all the other potentials reaching the OPAmp into the same direction and if you don't violate the absolute maximum ratings.

    Can you show us a schematic?

    Kai
  • Toshiyuki,

    I presume your pin numbers (4 and 11) refer to a quad version, OPA4376.  Since there is no internal ground in any of our modern parts, including OPA4376, you may shift supplies anywhere you want as long as the total supply voltage, Vsup_tota l= (V+)-(V-), meets the minimum of 2.2V and maximum of 5.5V specifications listed in OPA4376 datasheet.

    Of course, as you shift the supplies, the input common-mode and output voltage ranges, which are defined with respect to supplies, must also move accordingly; therefore, for -5V to 0V supplies, Vcm and Vout linear ranges would move to: -5.1V<Vcm<0.1V and -4.95V<Vout<-0.05V, respectively - see below.

    I have simulate the circuit for buffer configuration - see below:

    Toshiyuki OPA4376.TSC

  • Toshiyuki

    We haven't heard back from you so we assume this answered your question. If you need additional help just post another reply below.

    Thanks
    Dennis