I have a customer asking for the dimentions to the OPAMPEVM-SOIC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a customer asking for the dimentions to the OPAMPEVM-SOIC
Hi Devon,
We don't have the SOIC EVM version on hand, but we are pretty sure the outer dimensions for the SOIC and PDIP boards are the same. Measurment of the PDIP board produced dimensions of 132 mm (X) and 127 mm (Y). Keep in mind that the boards accommodate single, dual and quad versions of op amps, and there is a lot of space for other components. That is why the boards are rather large.
Regards, Thomas
PA - Linear Applications Engineering