Using a multimeter on Pin 1 and 2 of OPA2541SM, the table below shows results on 3 separate units
Test Condition 1 |
Test Condition 2 |
Test Condition 3 |
Test Condition 4 |
|
6(-Vs) |
6(-Vs) |
2(+Vs) |
2(+Vs) |
|
1(OutB) |
5(OutA) |
1(OutB) |
5(OutA) |
|
Pin Impedance value (?) |
200Kohm ↑ |
200Kohm ↑ |
1.2Mohm ↑ |
1.2Mohm ↑ |
Unit 1 |
321K |
319K |
1.47M |
1.51M |
Unit 2 |
290k |
217k |
1.39M |
1.25M |
Unit 3 |
301K |
310K |
19.5K |
1.4M |
I'm not sure what the "Pin Impedance value" is.
Is there an explanation for the discrepancy for Unit 3, Test Condition 3?
A value of ~1.4Mohm is expected , but the result is 19.5kohm. Out of 100 pcs, 2 units had these discrepant results.
Is it simply a faulty unit, or could there be another explanation?
Any help would be greatly appreciated...
Thank you