I need to drive multiple piezoelectric transducer at high frequencies(1MHz - 8MHz), but my function generator is not able to provide high voltage(ranging from 100-250v is needed for effective vibration amplitude). I am not sure what amplifier would be suitable for these frequencies, as this seems to be quite difficult to achieve. I would appreciate it if anyone could help me figure out what amplifier would be able to provide me with what I need.
Thanks in advance.