Welcome to the Audio Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TPA505XEVM GUI get stuck
HiWhen running the GUI, the I2C status light turn red most of the time. Need to reset the board, unplug and plug in the USB, and run the GUI, the I2C status turn Green.However, touching any of the buttons or changing any registers, the GUI simply get stuck, the reoccurrence is 100%.Have try numerous times, also with PC reset, same problem occurs.The GUI is downloaded from the product folder which is version 2.0
A: Re: TPA505XEVM GUI get stuck
It works after removing the J3-J5 corresponding to address 0.
Q: Re: TPA505XEVM GUI get stuck
Alternately, you could change the I2C address in the GUI.