Which Processor can be used exclusively as a GPU, only for driving the LCD

We are trying to build a touchscreen based LCD display with a minimum SVGA resolution (800 x 600). We are looking for a TI processor which can be used exclusively as a GPU, for driving the LCD. We found, that the Stellaris processors wont be able to drive this resolution. Sitara family processors are high end, and if used they would be under utilised. So, is it possible to use C2000 family processors to be used as LCD controller, I mean designing a GPU using C2000 processors. The application wont involve any high end graphics or video.