This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PGA450Q1EVM: GUI was frozen when opening

Guru 22490 points

Part Number: PGA450Q1EVM

Hi Team,

My customer got PGA450Q1EVM and I heard GUI was frozen when opening GUI.
I attached the picture after GUI was frozen.



His startup procedure is no ploblem according to the following E2E thread.
https://e2e.ti.com/support/applications/automotive/f/26/p/569058/2088597#2088597
1. Connect TI-GER board to EVM.
2. Connect and power EVM.
3. Connect USB from TI-GER to PC. 
4. Open GUI.

He also tried the following startup procedure to isolate the TI-GER board, however same freeze error can be replicated..
1. Only connect the TI-GER board to the PC (EVM should not be connected or powered)
2. Open the GUI. Does the GUI still freeze?

What is concern?

Best Regards,
Yaita / Japan disty

  • Yaita-san,


    I've moved this post to the Automotive Forum, where questions about the PGA450-Q1 have previously been posted. I'm sure that you'll find an answer here.


    Joseph Wu
  • Guru 22490 points

    In reply to Joseph Wu:

    Hi Joseph-san,
    Thank you for moving to the Automotive Forum.

    TI Automotive team,
    Could you please give me comments about the issue?

    Best Regards,
    Yaita

  • In reply to K.Yaita:

    Hi Yaita-san,

    I have assigned the appropriate engineer who should be responding to your question.

    Thanks & Best Regards, Scott
  • Guru 22490 points

    In reply to Scott Monroe:

    Hi Scott-san,

    I appreciate for your help. 
    I suspect it as the cause of defect of TI-GER board.. I also attempt to get another EVM in parallel.

    Best Regards,
    Yaita

  • Hi Yaita,

    Please try the following TI GER board reprogramming procedure:

    The procedure for reprogramming firmware preloaded in the TI GER over USB  allows updated firmware (*.HEX file) to be loaded into the microprocessor by executing the following procedure:

     1. Open HIDBootLoader.exe.

     2. With the TI GER connected to the USB bus, place a jumper in the “HEX” jumper location on the TI GER. The green LED will illuminate.

     3. Depress the RESET pushbutton. Now the boot loader mode is activated.

     4. In the HIDBootLoader program, verify that “Device attached” appears in status the window.

     5. Click the “Open Hex File” button, and navigate to the location of the *.HEX file to be uploaded.

     6. Once the file is selected, click on “Program/Verify”

     7. Wait for programming conformation, then remove the HEX jumper and press RESET button.

    Let me know if this procedure eliminates the GUI-freezing error. I am also attaching an older version of the GUI to determine if the error is due to a GUI update.

    Tiger Firmware update kit.zipPGA450 GUI 1.40.0.zip

    Akeem Whitehead // Texas Instruments // ASC-SENSING-SSC // Applications Engineer
    Visit our Ultrasonic Sensing FAQ page for additional information.
  • Guru 22490 points

    In reply to Akeem Whitehead:

    Hi Akeem-san,

    Thank you for your support.

     >1. Open HIDBootLoader.exe.
    Where can I get the HIDBootLoader.exe and *.HEX file?

    Best Regards,
    Yaita

  • In reply to K.Yaita:

    Hi Yaita,

    I attached the zip file containing the .EXE and .HEX to the bottom of my last message.

    I also attached PGA450Q1GUI version 1.4 in the bottom of the last message.

    Are you able to download both zip files?

    Akeem Whitehead // Texas Instruments // ASC-SENSING-SSC // Applications Engineer
    Visit our Ultrasonic Sensing FAQ page for additional information.
  • Guru 22490 points

    In reply to Akeem Whitehead:

    Hi Akeem-san,

    I apologize for having overlooked.
    I will try your procedure.

    Best Regards,
    Yaita

  • In reply to K.Yaita:

    Hi Yaita,

    Also, ensure that the HEX jumper pins on the TI GER board are not shunt-shorted. Should appear as follows:

    Akeem Whitehead // Texas Instruments // ASC-SENSING-SSC // Applications Engineer
    Visit our Ultrasonic Sensing FAQ page for additional information.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.