• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Applications » Automotive » Automotive Forum » designing a CAN interface for automotive ECU from scratch
Share
Automotive
  • Forum
  • E2E Wiki
Options
  • Subscribe via RSS

designing a CAN interface for automotive ECU from scratch

designing a CAN interface for automotive ECU from scratch

This question is answered
Daniel Sofer
Posted by Daniel Sofer
on Apr 23 2012 06:02 AM
Prodigy90 points

Dear Sirs,

I am working on a new automotive ECU design, which shall be used on heavy duty Diesel powered engines.

Among the features to build into it, one (or more) CAN interfaces are must.

Looking at scope readings from other ECUs, we can see that the actual voltages used are about 9V(low) and 16V (high) levels. Baud rates are fairly low, at 125k, for this specific application.

A quick look into TI's product range indicated the SN65HVDA542-5-Q1.

I would kindly ask if this selection is correct and what external components would be required to get the voltage levels we need.

This would allow us to start designing as we purchase the parts. As it is not unusual to any of us, this is quite urgent.

Thanks in advance,

Daniel Sofer

DSA

CAN SN65HVDA542-5-Q1
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • John Griffith
    Posted by John Griffith
    on Apr 23 2012 14:34 PM
    Expert4590 points

    Daniel,

    To start off, here is a comparison of the CAN devices that we offer. As you can see, depending on the low power mode you are looking for (standby, silent) and whether you are looking for a split pin or and I/O voltage level pin you will be looking at different devices. 

    HS CAN Device ISO11898-2 ISO11898-5 Low-Power State Wake I/O Voltage Split Pin
    HVDA1040A-Q1 Yes Yes Standby Yes 5 Yes
    HVDA1050A-Q1 Yes No Silent No 5 Yes
    HVDA540-Q1 Yes Yes Standby No 3.3/5 No
    HVDA540-5-Q1 Yes Yes Standby No 5 No
    HVDA541-Q1 Yes Yes Standby Yes 3.3/5 No
    HVDA541-5-Q1 Yes Yes Standby Yes 5 No
    HVDA542-Q1 Yes Yes Silent Yes 3.3/5 No
    HVDA542-5-Q1 Yes Yes Silent Yes 5 No

    The TXD and RXD pins can be interfaced directly with a micro, only requirement being that the pin that TXD is attached to has an internal pull-up resistor. If this is not the case then an external pull-up is required since the TXD pin is open drain.

    For the most part the only other design considerations that need to be considered are the type of external protection that you want to provide on the CAN bus pins. These protection schemes can vary from OEM to OEM. Below is a picture of a genaric CAN EVM that we have that enables uses to choose between have chokes, diodes, caps in different areas on the bus. 

    John

    CAN Protection
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Sofer
    Posted by Daniel Sofer
    on May 10 2012 14:48 PM
    Prodigy90 points

    Dear John,

    I've had problems posting this reply, so I hope this one goes through.

    Low power mode is not a concern for our design, we shall shut down the ECU when engine is off, so just about any behaviour would fit our needs.

    As fas as protections are concerned, they may need to be tested, and for that much please point me to the link for the EVM you mentioned, should it be possible to purchase one.

    We shall certainly be working at 5V for I/O.

    As for split, what are the advantages?

    However, what I still have not understood is how the actual CAN bus voltages are generated. On the real, existing vehicle CAN bus (a heavy duty Diesel vehicle, with 24V electrical system) the CAN bus voltages are +9V (low) and +16V levels are generated. These are the voltage levels I must have in the CAN bus because our system will be plugged into the existing CAN bus.

    Thanks in advance,

    Daniel

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • John Griffith
    Posted by John Griffith
    on May 11 2012 15:16 PM
    Expert4590 points

    Daniel,

    Unfortunately the EVM I was mentioning is not yet released, but we could work something out to get one populated in shipped to you if needed.

    The split pin offers some bus stabilization. The combination of the output 2.5 volt supply,  and the resistors and cap which make a low pass network, will help remove high frequency noise on the bus.

    What I do not understand it "the CAN bus voltages are +9V (low) and +16V levels are generated". A CAN bus has the following characteristics:

    Our tranceivers are designed to hold the bus recessive at 2.5 volts and have the dominant state create a ~2volt differential signal centered around 2.5volts. Please provide me more information on the CAN bus for your Deisel Truck application and I can be of more assistance. 

    John

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Sofer
    Posted by Daniel Sofer
    on May 23 2012 07:02 AM
    Prodigy90 points

    Hi John,

    As far as the EVM, it would be of great help, of course. But maybe we can just work things out via posts and just select the correct component and proceed directly to making our own PCB, even if a development one to start with.

    Now, as for voltage levels: Indeed the physical reality of the CAN busses I've come across in heavy duty vehicles has quite different voltage levels than those you mentioned, most likely to withstand electrically harsh environments. The actual waveforms are something like this:

     

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Sofer
    Posted by Daniel Sofer
    on May 23 2012 07:08 AM
    Prodigy90 points

    For some reason the waveform pic did not get posted. Here it is:

    Apparently this is according to ISO WD11992-1.

    All real life readings I've come across are +9/+16V.

    Cheers

    Daniel

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • John Griffith
    Posted by John Griffith
    on May 30 2012 13:30 PM
    Verified Answer
    Verified by John Griffith
    Expert4590 points

    Daniel,

    This is the first time that I have seen CAN bus voltages at these levels. TI does not offer any devices capable of this. We have some 3.3 volt and 5.0 volt CAN transceivers. 

    3.3 volt bus levels:

    5.0 volts bus levels

    Thanks,

    John

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use