Dear,
I am working on design using ultrasonic sensors that can be used to detect the distance (20cm- 1.5m) between moving cars and wonder to have answer to the following questions if possible:
- From you experience which ultrasonic sensor company is best to choose from?
- Which processor or controller for best to use?
- Do you have an application note that I can refer to that help my design?
- To use ultrasonic senor in harsh environment such as vibration, rain, snow, etc. is there a specific standard ultrasonic sensor must meet?
Thanks,
Bishara