Please explain the maximum output resistance parameter listed in Table 4-3 on page 28 (SLVSBC4A, December 2013), and also, note (1) below the table?
Is the maximum output resistance specifying the output resistance internal to the TPS65381-Q1 for the DIAG_OUT pin when AMUX is enabled? If not... what is the parmater specifying?
It's not clear to me how to use this information.
Ultimately, I'm trying to connect the DIAG_OUT pin to both and analog input and a digital input of an RM48L952 for diagnostic purposes in a safety application. Any application recommendations would be helpful (example schematic for example).