Hi, team,
For TPS65320-Q1, is it designed only for BUCK output higher than LDO application when both are on, as below operation mode ‘’EN1=1, EN2=1’’ ?
Now customer want to set the LDO output at 5V, and the DCDC output is 4V, but it seems the LDO output is only right when BUCK is disable. When both BUCK and LDO are enable, the LDO would follow the output voltage of BUCK ?
Also, in the spec of page 18, it mentions there is one charge pump for LDO, but I don’t see it in the block diagram and what is its function?
Besides, do we have another one Buck+ one LDO part that have completely independent enable signal to realize the application above, not like TPS65320-Q1?