Hi
For LM2904, I 've seen 0.7mA(TYP) at V0=2.5V with no load as shown in below.
If you have a current spec with below condition would you share with me?
Vo=0V, No load
Hope to see prompt answer.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
For LM2904, I 've seen 0.7mA(TYP) at V0=2.5V with no load as shown in below.
If you have a current spec with below condition would you share with me?
Vo=0V, No load
Hope to see prompt answer.
Thanks in advance.
You should post the conditions for the input and supply rails.
An amplifier with a 5V supply biased to a 2.5V output is no different than an amplifier with a +/-2.5V supply with a 0V output. This assumes the inputs are biased accordingly in each scenario.
The LM2904 includes 0V for the low end of the common mode range. The output low voltage is a few mV, so not *exactly* 0V.
Should the presumption be: Configuration buffer, Vin = 0V, Vout = ~0V, Vss = 5V, Load = open?
-Ken
Hi Jake if you could further clarify as asked and in parallel I'll see if there is any other data over the next day or so.
- Scott
Hi TIers
Below is my actual condition. If you don't have the test data for my case.
Let me have similar test data or if you can, let me have all test data.
Vcc = 12 ~ 14V (Normal : 12.5V) , GND = 0V
2. IN-, IN+ = 0V
3. Load = Open
4. Out = ~0V
Thanks.
Jake,
We could look at one unit for a typical value if that is what you mean. We cannot perform additional multi-lot qual or characterizaiton if this is what you mean by different LOT.
Please clarify.
- Scott
Hi Scott
In your reply, I guess you don't have test data, right?
I was asking to test multi-LOT. However, It should be appreciated if you test just one sample.
Thanks for the reply.
Hi Jake,
I took typical data for a single unit under those conditions in the lab. Icc may be summarized as:
Vcc | Icc |
12V | 0.513mA |
12.5V | 0.517mA |
14V | 0.531mA |
- Scott
Hi Scott
First of all, Thank you for the data.
Additionally, Can you provide the lot number of the sample what you tested?
Thanks and best regards