Dear, All
The absolute-maximum-rating value of the output pin of TPS7A6650-Q1 is 7V.
Input power source resisting pressure is a low value to other products and products of the other company as LDO beyond about 40V.
(For example, TLE4275-Q1 is 16V.)
I would like to know the reason.
For example,
- In order to reduce - chip cost?
- A protection circuit is added which does not occur [ emitting smoke ] even if an internal sense circuit breaks down?
Please teach me the above reasons.
Thanks, Masami M.