This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Output-voltage tolerance of TPIC74100-Q1

Other Parts Discussed in Thread: TPIC74100-Q1

Dear, All

The following questions are coming from the customer.
- Output-voltage tolerance
  Conditions, Vdriver 1.5V to 40V, full temperature range
- Standby current MAX
  Conditions, Vdriver 1.5V to 40V, ENABLE = low, full temperature range
Although the value at the time of 6V to 17V has Vdriver in a datasheet, they are not the above-mentioned conditions.
Since it is not necessary to be a guaranteed performance, I want you to teach.

Thanks, Masami M.