Hi Clancy ,
I have written 4bytes in EEPROM then I want to read those values and need to update in array. It is written in EEPROM read through GUI.
I havedone in following way:
unsigned char xdata EEPROM_BANK0[16] _at_ 0x0000;
Write(Loc,Value);
Read(Loc);
Read(Loc){ for(i=0;i<4;i++){ readArray[i]=EEPROM_BANK0[i]; }}
for(i=0;i<4;i++)
{
Localarray[i] = readArray[i];
}
1)Is required time delay between after EEPROM write to read EEPROM values.
2)Is required time delay between each location read?