I would like to conifrm the output capacitor for LP2951-50-Q1.
1. I attached the file for the circuit.
I think the output capacitor is OK, but I'm afraid the use of low ESR capacitor for bypass capacitor
of other (connecting) IC. Are there any problem of this circuit?
2. The output capacitor requirement are >3.3uF and the ESR 30mohm - 5 ohm. Is this correct?
Are there upper value of the capacitance (ex. 100uF, 330uF and so on)?
3. If you can, could you provide the first pole and second pole frequency (P1 and P2 of the file I attached) ?
Best regards,
Atsushi Yamauchi