Hi
Please let me know the action of TPIC6C in the following conditions.
Usually, LED is driven with 5V power supply TPIC6C596.
Power supply voltage descends to 2.7V for 10 ms.
In the meantime, can an output be held without malfunction?
When there is communication from a microprocessor on the same conditions, how is it?
It is satisfactory, if a function is lost in 2.7V and an output is turned off and fixed.
How is it at 3.7V?
somewhere has threshold value voltage -- please let me know.
Thanks.