I would like to confirm the output voltage of LP2951-50-Q1.
In the datasheet, the specification of the accuracy is +/- 2% with IL = 100uA.
I have a question.
How much is the accuracy with IL = 100uA to 100mA?
I think the accuracy depends on the output capacitor value.
When the output capacitor is 100uF, how much is it we can estimate?
Best regards,
Atsushi Yamauchi