I would like to confirm the failure mode of TPIC6B596 with the battery-OUTPUT short condition.
When INPUT is not incertitude (OUTPUT is not "L") and OUTPUT(Anode) shorts GND, TPIC6B596 is broken by the over current. Is this correct?
If it is correct, I have questions.
1. What is the condition of IC after the crash? Is it "Short" or "OPEN"?
2. When it is broken, does the smoking or the ignition occur?
3. After it is broken and the short conditon continues, does the function of IC stop?
Or does the smoking or the ignition occur?
Best regards,
Atsushi Yamauchi