DRV3201-Q1 About Programmable Dead Time function
Hi
My customer is using DRV3201-Q1.
Could you let me know about the following?
- I understood that this function detects time between the high input voltage of IHSx and the high input voltage of LHSx.
and If the time of input is short than setting time, DRV3201-Q1 outputs of GHSx and GLSx are to become low voltage during setting time.
Is my understanding correct?
- In datasheet P19 "IHSx/ILSx Outputs (Programmable Dead Time Disabled)" and "IHSx/ILSx Outputs (Programmable Dead Time Enabled)",
I think that GHSx/GLSx is correct. (IHSx/ILSx is incorrect)
Is my understanding correct?
Thanks
Shimizu