Hello,
Q1
Please tell me the MAX level of the overcurrent limit of TPS57114.
Q2
Please tell me the MAX level of the overcurrent limit of TPS54388.
Best Regards,
Kei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Q1
Please tell me the MAX level of the overcurrent limit of TPS57114.
Q2
Please tell me the MAX level of the overcurrent limit of TPS54388.
Best Regards,
Kei
Sato-san,
Q1
The max we have seen in the char data is ~7.3A
Q2
The max we have seen in the char data is also ~7.3A
Hello Alex,
Thank you for reply.
TPS57114 and TPS54388 are different in current value.
Therefore I think MAX value of current limit is also different, how about you?
Best Regards,
Kei
Sato-san,
The average current limit threshold in the datasheet is:
6.4A for the TPS57112-Q1 and
6.5A for the TPS54388-Q1
So I do believe it is reasonable for them to have the same maximum current limit threshold of 7.3A.