Dear all,
My customer want to drive the following three types of speaker by TPA3110D2-Q1.
【Three speakers】 *One IC drive one type of speaker.
・10W、16Ω x2
・12.5W、4Ω x2
・5W、4Ω x1
【Questions】
1. How much does this device can drive output power at 16Ω speaker? (??W@12V,16Ω,10%THD)
If possible, I want typical characteristics graph about 「Resistance vs Output Power 」.
2. I want to know about output power at various supply voltage.
I want to know about output power at 8V/10.6V supply voltage@16Ω/8Ω/4Ω.
If possible, I want typical characteristsics graph about 「Supply voltage vs OutputPower」.
3. If I use this device under 0.6W output, is there concern about this?
(Can this device output? Is efficiency down?)
4. I would like to know about concern to use same IC for three types of speakers.
(Can TPA3110D2-Q1 drive three types of speaker in the first place?)
Best regards,