Hi all
Would you mind if we ask LM2901-q1?
We use LM2901AVQPWRQ1 as attached file.
(please refer to following file)
20150128_Attachement.pdf
<Question>
The characteristic(typ) of LM2901's overdrive shows on the datasheet P9.
Is the characteristic of LM2901-q1's overdrive the same as LM2901's one?
And then, we use IN+(0.1V) and IN-(0.2V / 0V) within Vicr.
In this case, Is "TYPICAL CHARACTERISTICS (continued)" the same as the datasheet?
(Because, IN+, IN- are close to GND, so we would like to confirm these.)
Kind regards,
Hirotaka Matsumoto