Hi Clancy !
We are working on Pga450q1. My module is not working. I am attching the screenshot of error.(DEVRAM NOT SUCCESFUL)
I will write you all the steps taht i have done..!
1)Attach TIGER Board to PGA450Q1EVM.
2)Apply +12 volts to VPWR-IN and GND banana plugs.
3)Plug the TIGER board into computer via USB cable.
4)Connect an oscilloscope probe from Channel 1 to the TESTO_A test point on the EVM. and other end to ground. of board.
5)Place micro into reset by clicking on the “Off.
6) click on the “Check OTP Status and it was empty.
7) “Program OTP Memory Also” box checked in the “DEVRAM” tab, and supply 8V on VPROG OTP pin by installing the VPROG_OTP
jumper, and connecting the (8V) and VP_OTP pins.
8)Load .HEX File into GUI” button on the DEVRAM tab.
Here I got the error..!
I haven't done anyyhing with respect to EEPROM..!
Its reaaly urgent please tell me my mistakes in these many steps and if there is something that i haven't done.