hey..!
My DEVRAM has been programmed succesfully..
AFTER that the steps that I have performed.
1)Disconnect the (8V) and VP_OTP pins.
2)On the Evaluation tab, click on the “Amplifier Output (unfiltered)” button.
3)Release the micro out of reset by clicking on the “ON
4) In the LIN tab, receive a LIN transmission by clicking “RECEIVE” with PID = 21 and Number of
bytes to be received = 2..
and there should be 0x(1234) This verifies that the
firmware is loaded properly and that the GUI is communicating through LIN with the PGA450.
But I am not getting anything ...
Please solve my problem..its urgent..
Thankyou..