I'm working with the TPIC71002-Q1 (dual channel squib driver IC) and the datasheet references a Storage Capacitor connected to the VZx pins (pins 22 and 27). Is this a true capacitor or just a reference to the power supply that provides the VZx pins with the voltage for the squib loops? If the VZx pins do require a storage cap in addition to the power supply line to operate, could someone recommend a suitable capacitor value? I've attached a picture from the datasheet below for quick reference. I'm pretty new to working with squibs so any advice would be appreciated.
Thanks!