This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A6350Q question

Dear all.

1. According to datasheet p.6 pin function, nWD_EN pin has internal pulldown resistor.

   How much is the pulldown resistor?

2. According to datasheet p. 4, What is mean  5.25< Vdd < 3V at parameter of wachdog enable InpuT & Input pulse ?

Best regards.

  • Mike,

    The appropriate applications engineer has been notified of your inquiry, and will respond accordingly.

    Regards,
    Eric Hackett
  • Hi Mike,

    1. There is not a real resistor inside the TPS7A6350-Q1 nWD_EN pin, but an active device to realize resistor function. If 5V voltage is applied to nWD_EN, the current consumption is 0.5uA~8uA @-40<TJ<150C.

    2. Please ignore it, this was written by mistake as there is no Vdd pin. We will update this datasheet soon.

    Best regards,
    Jason Liu