Hi,
TPS7B6701-Q1 has 12 NC terminals.
Is there the terminal connected to the internal circuit in these pin ?
I need this information to consider the short mode between terminals.
Thanks and Regards.
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
TPS7B6701-Q1 has 12 NC terminals.
Is there the terminal connected to the internal circuit in these pin ?
I need this information to consider the short mode between terminals.
Thanks and Regards.
Kuramochi
Hi,
I understood there is no connection between the NC pin and internal circuit.
Does it mean it is possible to connect NC pin to Vin(40V) or GND?
I believe it is no ploblem but would like to confirm just in case.
My customer is considering FMEA(failure mode effect analysis) for this device.
Best Regards,
Yaita / Japan disty