Hello,
My name is Chentao and I am using TPIC8101 for knock detection. I have read the TPIC8101 manual many times, but there is not enough information about the bandpass filter. So I come here for help. I will be appricate if anyone can help me.
1 First I want to confirm one thing, the Q-factor. See the following website:
John Griffith said that the Q-Factor is 2.3, but I have heared that the Q-Factor is fixed to 2.5. So I want to confirm which one is right.
Is there any method to measure the Q-Factor?
And why the Q-factor is fixed?
2 The detail information about the bandpass filter. FIR or IIR, the filter order, and the type: Direct Form I or Direct Form II or other type?
3 About the coefficients of the bandpass filter.
As far as we know, the center freqency of the filter can be configured from 1.22KHZ to 19.98KHZ, so there are maybe 64 coefficient sets in the TPIC8101. Where are the coefficient sets stored? Does the TPIC8101 has its own ROM to store the coefficient sets?
Or the coefficients are calculated by the TPIC8101 due to the center frequency configuration?
4 About the transfer function of the TPIC8101. See the following picture: Because w = 2 * pi * f, so we should use Vin = VIN * sin(2 * pi * Fbp * t). But in the TPIC8101 manual, it always use Vin = VIN * sin(pi * fbp * t), why? Is there something wrong?
5 About the calculation of the tc. Tc is typically Tint / (2 * pi * Vout). But how do we get this formular?
That is all, waiting for your reply and best regards